(0)| 8/31/2014 3:56 PM | |
|
Posts: 6 Rating:
|
|
Last edited by: KhanhLee at: 8/31/2014 3:57 PM |
|
| 8/31/2014 6:16 PM | |
|
Joined: 11/21/2007 Last visit: 1/8/2026 Posts: 2327 Rating:
|
Hello KhanhLee The Profibus communication with MM4 drives can consist of 2 parts a) PKW -> For Reading / Writing Parameters b) PZD -> For Reading Actual Values & Status Words / Writing Setpoints and Control Words You can download the Manual of Profibus Module for Micromaster Drives from here : Operating Instructions: MICROMASTER PROFIBUS Optional Board Please go through the Section 3.4 : PKW Mechanism for Reading / Writing Parameters. I think this will provide you with all the details you need to Read / Write parameters from MM4 drives. Hope this helps Cheers Navnag |
|
There is no such thing as the last bug in a program |
|
This contribution was helpful to
|
|
| 9/1/2014 12:56 AM | |
|
Joined: 9/27/2006 Last visit: 1/12/2026 Posts: 12480 Rating:
|
Hello KhannLee; In addition to Navnag's important information, have a look at these FAQs and discusiions on the subjet of PKW mechanisms. MICROMASTER 4 (MM4): What is important when setting up an MM4 with a Profibus module? MICROMASTER 440 DP The configuration of the drive over 4PKW Notice that: -you must select a PPO x appropriate for both PKW and PKZ integration in the Profibus-DP telegram, so try PPO1,PPO2, or PPO5 (see the second link above). - the telegram you set up fpr PKW evaluation must be continuous over the 4 WORDs to be transfered, which means yoiu must use SFC 14 and SFC 15 to exchange the data between the CPU and the drive. See the sample projects in the first link. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/6/2014 4:25 AM |
|
This contribution was helpful to
|
|
| 9/21/2014 1:46 PM | |
|
Posts: 2 Rating:
|
Hi, My explanation in this topic may help you. https://www.automation.siemens.com/tf/WW/en/Posts/93275 |
Follow us on