Industry Online Support
Technical Forum
11/2/2014 10:27 AM | |
Posts: 2 Rating: (0) |
Hi, everyone! I am beginner user of Simatic S7. Can anyone help, I have problem with Cyclic Interrupt, I use CPU 315, I read above that Cyclic Interrupt time has to be more than than the longest PLC cycle time. I set 100ms(by default), And changed the Cycle of OB1 from 150ms to 50. Anyway, both my OBs (OB1 and OB35) runs in one time, has no any interruption ------------------------ New subject after splitting from additional cyclic interrupt. |
Last edited by: Min_Moderator at: 11/3/2014 1:58 PMSplitted |
|
11/2/2014 2:55 PM | |
Posts: 8946 Rating: (999) |
That is completely WRONG. |
Follow us on