(0)| 12/2/2014 10:02 AM | |
|
Posts: 1058 Rating:
|
You did not state anything about hardware and software used in your configuration and weather you use it as Master or Slave. So have a look here at FAQs for Modbus RTU: Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol? How do you establish a MODBUS-RTU communication with STEP 7 (TIA Portal) for the SIMATIC S7-1200? How do you download a loadable driver such as "Modbus Master (RTU)" into a CP341 that is connected to an S7-400 H system by means of an ET 200M? Modbus RTU Communication Module Manual, Modbus master software, Modbus protocol regards |
Follow us on