12/11/2014 6:26 PM | |
Joined: 3/19/2012 Last visit: 6/6/2024 Posts: 18 Rating: (1) |
hi, I faced similar issue. I was able to generate module driver connection for digital input and output. But not for analog. When I deleted the symbol from symbol list and generated again, I got those connection. After that I added to symbol table and then it was still there. But this was very intermittent. It dint work for other I/Os ------------------ New subject after splitting from PCS7 Warning Compilation - "No hardware found for symbol XXX whith address compilation XXX". |
Last edited by: Min_Moderator at: 12/12/2014 10:41 AMSplitted |
|
12/15/2014 8:09 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
It could mean that you configured analog cards are not support by your pcs7 version. The system cannot generate the analog drivers because there are not known to the system. This could also be that you are using newer versions that is not in your hardware catalog. We have this problem for our customer which still uses pcs7 6.1. When expanding the plant with hardware, we use the newer version of the SM321,323,322 family, because the old ones arenot manufactured anymore,howeverthe new version does not exist in the hardware catalog because it's 6.1. Therefore no drivers can be generated. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on