(0)| 12/18/2014 9:07 AM | |
|
Joined: 12/28/2011 Last visit: 9/23/2025 Posts: 6 Rating:
|
Hi, I am using a Panel PC (IPC577C 15" Touch PN/IE) with Windows XP and WinCC Runtime Advanced v12 SP1. This is working OK. Our customer are now requesting to run a web server application on this HMI in order to use a web client (remote HMI) on a workstation located far away. Can we use the Web navigator server for this? Is it suitable with the current configuration on the Panel PC? Hope for quick response, thank you! ---------- New subject after splitting from Wincc v13 web navigator. |
Last edited by: Min_Moderator at: 12/18/2014 2:42 PMSplitted |
|
Follow us on