(0)| 12/25/2014 1:15 PM | |
|
Posts: 84 Rating:
|
Hello everybody; I want to ask a question about FM350-2 it is related with observing the physical output of the high speed counter card "Q0". It looks like DBxxx.DBX22.0 in its manual as CONTROL_SIGNALS.SET_DQ0. In our project, related DB is DB30. however, when I put DB30.DBX22.0as triger input of a counter, I can not see any change on counter.. An expert told me that"you can watch it from DB30.DBX42.0 as CHECKBACK_SIGNALS.STS_DQ0"this is working for counter. But I want to see if it is physicallytriggered or not. Is it possible to observe that signal directly or STS_DQ0 is the only way to see it??? -------- New subject after splitting from Direct Access of FM350-2. |
Last edited by: Min_Moderator at: 12/26/2014 12:42 PMSplitted |
|
Follow us on