(0)| 12/29/2014 12:47 PM | |
|
Posts: 8 Rating:
|
we have same problem with IM154-8FX PLC when using the motor starters. we have about 10 control systems with SAMEhardware as well as software configurations. out of this10 systems has 5 systems gots the problem "PROFINET IO module removed/cannot be addressed" for slot number 11 consistently. for other 5 system it for slot no.12 consistently. the fault gets automatically reset in few miliseconds. below are the diagostic buffer history. Event 1 of 10: Event ID 16# 3854
PLC version simatic manager 2010 ver5.5 sp3. starter module part number:- 1.3RK1304-5LS40-4AA0 2. 3RK1304-5KS40-5AA0 we already checked all earthing and related possiblity of fault. every thing is OK. pls suggest what may be the issue. Chetansing Patil ---------- New subject after splitting from Identify if the bus back plane connector of s7-300 is working or not?. |
Last edited by: Min_Moderator at: 12/29/2014 1:03 PMSplitted |
|
| 1/5/2015 12:06 PM | |
|
Posts: 8 Rating:
|
pls suggest! |
Follow us on