Industry Online Support
Technical Forum
1/28/2015 3:19 PM | |
Posts: 1 Rating: (0) |
Dear All, I have very similar problem. I have a hardware configuration: TP177A + S7-300 (CPU315 2DP) + robot COMAU all connected via profibus. The problem is with sending/receiving signals to robot Hardware configuration is compiled with no error. I uploading some OB (OB1, OB86, OB122) block to S7-300. In OB1 block, I have put 1 network PIB5 - MOVE - MB0 and after upload it to S7-300, SF is red. In Module information I have error access reading OB122 (please find attached file). Removing network 1, everything is ok, S7-300 is green, I'm sure that I have communication with COMAU because when the robot is off I have error BFUS is blinking on red. When the robot is on everything is green. Alsto in hardware online everything is ok. Can any can help, what's is going wrong? where is the problem? Why I can't receive any data from ROBOT COMAU? -------------- New subject after splitting from I / O Access error. Attachment28012015.zip (178 Downloads) |
Last edited by: Min_Moderator at: 1/28/2015 4:04 PMSplitted |
|
1/28/2015 6:03 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello, There are some points regarding your problem:
In this case, at least your "I/O access error "problem will be solved. Best regards, Hamid Hosseini |
Last edited by: hdhosseini at: 1/28/2015 6:37 PMLast edited by: hdhosseini at: 1/28/2015 6:37 PM |
|
Follow us on