(0)| 10/19/2007 7:39 AM | |
|
Posts: 133 Rating:
|
Hi, Here are the logs from C:/Program Files/Siemens/WinCC/Diagnose. The logs are for a new project made on the target PC. On the target PC I was not able to start the Runtime. With Project Duplicator I have made a copy and tried on a test PC. On the test PC the Runtime started fine. I have the same WinCC installed on both PC. On the test PC (where the Project is working) I have other programs, like Nero, Office, Antivirus, etc (programs for every day use) If you see something util in the log files, or you know other diagnosys files wich I can verify please tell me. PS. I have tried to attache the project, but is bigger then 1MB. If you think it would be usefull for diagnose to tri the project you can download from here: http://automation.ro/~bszabolcs/WinCC/Test_Duplicate.zip AttachmentDiagnose.zip (140 Downloads) |
| 10/19/2007 10:12 AM | |
|
Posts: 3 Rating:
|
hi, have you ever installed Patch 3 that was released last month. This would solve your problem of graphics runtime getting struck at 77%. Before you install Patch 3, you need to completely stop WinCC application and all related services, restart the PC and then install Patch 3. You can download from the link below, http://support.automation.siemens.com/WW/view/en/25869221 Gopal |
Follow us on