(1)| 12/16/2007 7:21 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Jom, It is also possible to use a Diagnostic Repeater as a Repeater, it is a two in one repeater, so you come with one segment to the repeater. On that segment you could place another 30 Profibus Slaves. From the diagnostic repeater you have two other segments where you could place on both segments another 31 Profibus slaves. With this diagnostic repeater you could also do some diagnostics as the name would guess.. See for more information the handbookSIMATIC Diagnostic Repeater for PROFIBUS-DP 6ES7972-0AB01-0XA0 Diagnostic Repeater for Profibus DP |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on