2/26/2008 10:51 PM | |
Posts: 8 Rating:
|
Hello, Is there a way to keep the back light on the main display ON all the time?Programmatically or by setup? |
2/27/2008 7:30 AM | |
Joined: 4/6/2006 Last visit: 6/24/2025 Posts: 604 Rating:
|
Hi, No this is not possible. |
Best regards, |
|
2/27/2008 8:56 AM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hello, it is only possible, if you manipulate the LOGO! hardware and without any guarantee !!! A solution to do this is writen in the german part of the forum: Displaybeleuchtung ...>> LOGO-DISPLAY.pdf You must connect two wires (red!!! in the picture) insite the LOGO! basic module and find a way out of the module (that´s easy). Then you can get a external key or a LOGO! relay (!) output to control theinternal bachlight ON/OFF. But i think you shoud control the ON-time per logo circuit (and an external key) and NOT let the LED´s "ON" all the time! Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
2/27/2008 9:20 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear Curious, Let's wait till the new Logo will be released Best regards, Wizard |
6/28/2008 10:43 AM | |
Posts: 3 Rating:
|
Is this correct? Connect the two pads as indicated by the red line Connect two wires to the pads as indicated by the yellow lines Drill a hole in the PCB and route the wires out of the LOGO Connect the wires to a suitable external switch Is there any reason (thermal issues?) why I couldn't just use a three way connection between all three pads giving a permanent backlight? |
3/27/2020 6:04 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by dsn11 is split to a separate thread with the subject How can generate a new subject?. Best regards |
Follow us on