(0)| 5/9/2008 1:25 AM | |
|
Posts: 3 Rating:
|
i cannot find firmware cp 342-5 version v5.2 on the internet help? i want to do a simple digital I/O with profibus-DP anwith cpu314-IFM V1.1{6ES7 314-5AE03-0AB0} , cp 342-5 v5.2 {6GK7 342-5DA02-0XE0},ET200S {IM151-1 standard} , but LED "SF" and "BUSF" on cp is on i think it accosiated tocp version that thein simatic configured as v5.0 but the cp version is v5.2 andi attach project too see it complete. please guide me thanks. Attachmentprofibus simple IO.zip (529 Downloads) |
Last edited by: station300 at: 5/9/2008 10:09 AM |
|
| 5/10/2008 1:58 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Einstein, The versions in STEP7 are not mandatory, so I think it is not the way why some things are not working now. The newest version is also working with an older CP-version from STEP7 Hardware configuration. Firmware V5.7 for CP 342-5 / CP 342-5 FO |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on