(9)| 5/25/2008 9:30 PM | |
|
Joined: 4/6/2006 Last visit: 11/21/2025 Posts: 604 Rating:
|
Hi, I just wonder or you checked the Compatibility list for WinCC v6.2 SP2. Because that list will tell you that SP3 is not supported for WinCC. So this will cause the problems for sure. http://support.automation.siemens.com/WW/view/en/21927773 The best thing to do is reinstall your system with XP SP2. THis is better then just deinstalling SP3. |
|
Best regards, |
|
| 5/26/2008 9:43 AM | |||
|
Joined: 2/20/2007 Last visit: 1/7/2026 Posts: 18 Rating:
|
OK But no solution, since in new computers and automatic updates of the XP is installed SP3. Best regards, |
||
| 5/27/2008 10:48 AM | |
|
Posts: 1776 Rating:
|
Hi, sorry this update is not a part of SP3 see FAQ http://support.automation.siemens.com/WW/view/en/22016868 see also http://support.automation.siemens.com/WW/view/en/22531371 and shure the compatibility list |
| 6/17/2009 4:27 PM | |
|
Posts: 2 Rating:
|
Hi, It should just be a case of adding the folders (keys)manually into the Registry. Hope this helps. Jon |
| 6/17/2009 7:43 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Did you tried with uninstall of SP3 of Windows? How look at http://support.automation.siemens.com/WW/view/en/31694896 The right decision you already received from INS - frech copy of Windows XP SP2. Success and regards Hristo Mihalev |
Follow us on