(0)| 7/11/2008 12:10 AM | |
|
Joined: 1/25/2006 Last visit: 1/19/2026 Posts: 257 Rating:
|
Hi Lifrasil, I send you screenshot. When I make screenshot, the system was in offline. But, never mind, this alarm apperade when system is in online state. As you be able to see, in alarm fields (bellow of screenshot) appear the alarm which I can't solve in this moment. I tried to find mistake maybe in WDC receive command block is some problem. I haven't any idea. If you have some advices, please, send me. Thank you again. Zoran AttachmentScreenshot-Sinaut SC and Wincc flexible.zip (217 Downloads) |
| 7/17/2008 8:38 AM | |
|
Joined: 9/29/2005 Last visit: 12/2/2025 Posts: 313 Rating:
|
Hi Zoran, i guess the error message comes each time where the rhombuses are inside of the fields?! This can caused by a failure in WinCC flex or OPC Server or WDC_RECEIVE. WDC_Receive: Check the sequence of the blocks, must be: INIT,SEND,RECEIVE,CONTROL also check the settings of WDC RECEIVE as its described here: http://support.automation.siemens.com/WW/view/en/29737058 Take care of the parameter DATA_START and DATA_LENGTH If this won´t cause improvement then we have to take care of server and WinCC flex. But please give at first a feedback after checking WDC_RECEIVE. regards Lif |
Last edited by: Lifrasil at: 7/17/2008 8:55 AM |
|
Follow us on