(0)| 1/27/2006 7:28 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hello The PCAdapter USBfrom Siemens is working very well. [;)] Follow the link for more information: http://support.automation.siemens.com/WW/view/en/15315777 Best regards, Late |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
| 1/27/2006 7:53 PM | |
|
Posts: 4 Rating:
|
Thanks for the reply Late, any idea on what the cost of this beast is? Thats the scary part![:o] |
| 2/8/2006 9:45 PM | |
|
Posts: 3 Rating:
|
Hi! I think the problem is the power for the adapter. I had the same problem after our serialport broke. We bought an USB-Serial adapter and had communication with Mitsubishi PLC:s and e-900 panels and even OP-7 and MP-270. The big problem was with MPI-communication. Even thought the power-lamp did lit we couldnt communicate with the PLC. We bought a new laptop... Check: HMI Adapter (order number: 6ES7972-0CA1x-0XA0), PC Adapter (order number: 6ES7972-0CA2x-0XA0) and TS Adapter (order number: 6ES7972-0CA3x-0XA0) require both 5V and 24V at the MPI/DP interface. Siemens support say in this link : The following connections are not possible with a PC or USB adapter:
|
| 4/19/2006 5:27 PM | |
|
Posts: 62 Rating:
|
Greetings Berg, There are a number of them on the web. Google "PCMCIA to RS232" and they'll come up. Here's a link to the one we use: http://www.siig.com/product.asp?query=IO1037&pid=225 It's list price is $60.00 USD Best Regards Thumper |
Follow us on