(0)| 8/8/2008 11:10 AM | |
|
Posts: 1742 Rating:
|
Hello, Have a look in this manual on page 63: http://support.automation.siemens.com/WW/view/en/24432172 There is a specific poit: 11.6 What to do if you forget the password |
Last edited by: edr at: 8/8/2008 11:11 AM |
|
| 8/8/2008 12:29 PM | |
|
Posts: 3 Rating:
|
I've done it butI didn't foundfour digit code in TITLE tab of INFORMATION ABOUT MONITOR AND BUS. |
| 8/19/2008 4:57 PM | |
|
Posts: 25 Rating:
|
Dir Sir, A ""ONE TIME"" PASSWORD can be generated by the Technical Assistance of Siemens. Technical Assistance of Siemens need the present CODE of the Safety Monitor and a version > V1.x (both data are mentioned in the Safety Protocoll) The CODE is mentioned in the configuration protocol or can be get as follows: 1.) Disconnect the AS-i Cable from the Monitor. 2.) Stop the Monitor via the Software (Monitor-STOP). Without Password this is only possible if AS-i is not activated. Therefore: Set the Master to offline or disconnect the AS-i cable from the Monitor then give the STOP command. Make sure that the Monitor is in configuration mode (LED's show running indication). 3.) Get the configuration log. 4.) Get the CODE out of the protocol Next steps: a) Customer sends the CODE and the Monitor Version to Technical Assistance. b) Technical Assistance of Siemens generates a new Password for that special Monitor. c) TA forwards this ""ONE TIME"" password to the customer. d) Customer log in with this Password and changes the present Password to a new one. Description of the changing of the password: d1) Master setting to Offline or disconnect AS-i cable from monitor and then Stop Command type in. Check monitor is in configuration mode (running lights). d2) Command to change the password. - Old Password : type in new generated password e.g. 32610DD0. - Type 2 times new valid password in e.g. Hello. - After this you can work as before. After the changing of the configuration the code is changed and then the log in with the ""ONE TIME"" password is no more possible. After using the ""ONE TIME"" Password this Password is not longer valid. If it do not work pls. contact Technical-Assistance@Siemens.com Best regards |
Follow us on