(0)| 8/26/2008 7:17 PM | |
|
Posts: 3 Rating:
|
Hi All, Rsview 32SCADA system is unacceptably slow to operate and suffers from serious stability issues . The 2 SCADA Server System often fail to match up and will often lose communication with different areas of the plant for seemingly random intervals SCADA Machines Details :· Windows OS with Service Pack = Windows XP Professional Version 2002 Service Pack - 1· RAM =1 GB· Hard Drive Utilised Vs. Spare =C-Drive - 6.22GB / 9.98GB D-Drive - 9.15GB/101GB Software Versions Installed on SCADA machine :· RSView 32 Version=7.20.00 (CPR7)· RS Linx Version =2.51.00.21 (CPR7) System architecture: AB’s 4 SLC 5/04 and 1 SLC 5/03 Communicating on DH+ network with the Rsview 32 SCADA machine via PKTX Card Siemens 6 S7 PLC’s communicating on Ethernet network with the Rsview 32 via CP1613SCADA machine via lan Card over OPC Network Sattacon’s 7 PLC’s communicating on Satbus with the Rsview 32 SCADA Machine over stabus using stabus netwok adaptor. Please find attached system architecture file in zipped files. Windows System and application log Errors: Please find attached herewith System Log Files and Application log Files for your ready reference Could you please have a glance on the System event message -1.bmp and System event message -2.bmp snapshots ,asthis error keep on coming all the time and slowing down the machine . Your earliest response in this matter is much appreciated Thanks in advance. SVK AttachmentEvent Messages and Sys Architecture.zip (940 Downloads) |
Last edited by: SVK at: 8/26/2008 7:19 PM |
|
Follow us on