(0)| 10/4/2008 7:09 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hi No directly you can't connect OP. Read this FAQs: How is the connection between a Windows-based panel and a SIMATIC S5 set up? Connecting a Windows-based panel to the SIMATIC S5 (CP5431) via PROFIBUS DP Connecting a Windows-based panel to an IM308C (SIMATIC S5) via PROFIBUS DP Configuring communication to S5 best regards |
| 10/5/2008 8:23 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hi If you have TP270 you can connect AS511. Read here:http://support.automation.siemens.com/WW/view/en/1405528 See chapter 2. About MP277, i think you will need WinCC Flex not Protool and. You are right that this panel didn't have RS232. But with converter converter 6AV6 671-8XE00-0AX0 (RS 422-RS 232). More about MP277 look here. regards |
Last edited by: UMENCHO at: 10/5/2008 8:25 AM |
|
| 10/6/2008 9:43 AM | |
|
Joined: 4/24/2006 Last visit: 1/14/2026 Posts: 9105 Rating:
|
Dear rabbit, Please have a look at this manual: http://support.automation.siemens.com/WW/view/en/1405528 Chapter 3 will explain communication using AS511 protocol. Special function blocks for connection to the PLC are not required. The mentioned FB51 are for older panels. Best regards, Wizard |
| 10/10/2008 9:51 AM | |
|
Posts: 6 Rating:
|
thanks for your reply. I will try it to see the result. |
Follow us on