(1)| 10/16/2008 4:07 AM | |
|
Joined: 9/27/2006 Last visit: 12/23/2025 Posts: 12472 Rating:
|
Hello Roby; There is no specific area in the A&D forum for Desigop products, beacause they are a product of another Siemens division, the Siemens Building Technologies unit. Here is a link to the Desigo presentation page, on the SBT website. Some of us here have had occasion to work with these products though, so please ask; at least we will try to give you our best answer. Hope this helps, Daniel Chartier |
| 10/16/2008 10:47 AM | |
|
Joined: 9/27/2006 Last visit: 12/23/2025 Posts: 12472 Rating:
|
Hello Roby; A simple web search led me to this Desigo system description, where you can find the following information: Network gateways to DESIGO I/O, LONWORKS and KNX S-mode (EIB) Based on SIMATIC S7, Siemens Building Technologies offers an integration platform based on SIMATIC S7, for communication at the automation level. SIMATIC S7 is connected to the standard communications systems, LONWORKS and KNX S-mode (EIB) of the building automation and control system, by means of two network gateways, the DP/LON Link and the DP/EIB Link. This is the means by which the LONWORKS and KNX S-mode (EIB) field buses are integrated into PROFIBUS DP. In addition to the network access described, other means of access, such as the DP/AS interface link are also available. Gateway from PROFIBUS DP to DESIGO I/O The DP/P-bus link integrates the proven DESIGO P-bus input/output modules into SIMATIC S7. Within the SIMATIC system, the DESIGO I/Os (PTM modules) are treated as standard PROFIBUS DP data points and can therefore be accessed in the SIMATIC system. Gateway from PROFIBUS DP to LonWorks The DP/LON link integrates the LONWORKS bus of the building automation and control system into the standard communications system, PROFIBUS DP. For the individual room control range, DESIGO RX, the most commonly used applications are available for automated engineering. Gateway from PROFIBUS DP to EIB The DP/EIB link is used to connect the two open standard communications systems PROFIBUS DP and the building automation bus, EIB. The DP/EIB Link is especially designed for tasks associated with control of lighting and blinds in the context of the electrical installation. The construction of the device makes it suitable for installation in control panels and sub-distribution boards. They also mention Desigo SX Open, an OPC server with drivers to Profibus-DP. I don't have access to the actual part numbers of these gateways at this time, but if you need help locating them on the SBT website come back to the forum. Hope this helps, Daniel Chartier Edit: This document is in German, but in the last pages there are photographs of the gateways, and you can make out part numbers: DP/LON Gateway: 6FL 6301-1BA01 (Landis and Staefa part number) DP/EIB gateway: 6GK1 415-0AA00 (Siemens A&D part number) Hope this helps, D.C. |
Last edited by: dchartier at: 10/16/2008 11:11 AMNew information on Gateways to DP Last edited by: dchartier at: 10/16/2008 10:48 AM |
|
| 10/25/2008 2:13 PM | |
|
Posts: 22 Rating:
|
Help full Manual Desigo Xworks |
Follow us on