(0)| 2/5/2009 6:51 PM | |
|
Posts: 2661 Rating:
|
Hi vegas, Which version of PCS7/WinCCC are you using? What are the computer names of the ES, Sever & OS (client)? Regards |
| 2/5/2009 7:18 PM | |
|
Posts: 12 Rating:
|
Hi, |
| 2/5/2009 8:28 PM | |
|
Posts: 2661 Rating:
|
Hi vegas, AttachmentClientName.pdf (1132 Downloads) |
| 2/5/2009 8:43 PM | |
|
Posts: 12 Rating:
|
Display load log... 05/02/2009 01:37:46 p.m. : The entire WinCC project will be transferred to the runtime OS. |
| 2/6/2009 3:55 AM | |
|
Posts: 2661 Rating:
|
Hi vegas, There seems to be some confusion. 1. Can you explain what you mean by the following: Both server and clients should have identical user name and passwords. 2. The following has nothing to do with your problem. This is only for creating users in WinCC runtime like operator, supervisor etc.
3. The configuartion steps you have outlined are mainly if you are using native WinCC. With PCS7 many of the steps are automatically taken care. I suggest you use the PCS7 wizard and create a test project (including OS server and OS client) for better understanding. Let me know if youneed the step-by-step procedure. 4. Now, in your case it seems to be a network problem. Please check the following: a) Have you configured the lmhosts file properly (if you are using fixed IP addressing)? b) Can you ping your server from client and client from server using the computer name? c) Can you see the computers properly in Simatic Shell of each machine, that is, the terminal bus is properly configured. 5. The following FAQ's are very helpful. You should understand them very clearly. How can you clear the error message "Download (310:88)"? Let me know if you need any further help. Regards |
Last edited by: Phantom75 at: 2/6/2009 9:54 PMLast edited by: Phantom75 at: 2/6/2009 4:56 PM |
|
| 2/10/2009 6:47 PM | |
|
Posts: 12 Rating:
|
Hi phantom,
Date: 02/10/2009 time: 10:23:21 AM Refer to the log for the single objects for more information. I am desperate Attachmentjpga.zip (441 Downloads) |
Follow us on