(0)| 3/4/2009 1:18 PM | |
|
Joined: 3/21/2006 Last visit: 1/22/2026 Posts: 10248 Rating:
|
Hello OK. Let's try with your manual. (I found this is better). So, FB223 and FB224 enable you to transmit data using layer 2 services with minimal programming overhead. You only need to program these FBs once for an S5-95U. The FBs can be used for all layer 2 services. Look at SINEC L2 Interface of the S5-95U Programmable Controller (this is yours manual) page 151. For use in Step7 you need only number of DB. From this manual you can see - for each call of SEND or RECEIVE there has DB number (DBNR), start address (QANF), Send length (QLAE). In page 152 there have nice example. regards |
Follow us on