(0)| 4/3/2006 10:31 AM | |
|
Posts: 3 Rating:
|
thanks Thijsfor your reply i will describe my system in prife iwill make system for production data collection so i will use Touch panels in diffrent places in the shop floor to collect the production data in my design i will use one or two PLCs S7 300 to control the touch panels by connecting them with MPI network and i will connect the PLC to the pc by using CP 5613 to draw the data from the PLC to the PC i allready try to connect two touch panels to one PLC S7 and thePLC control them corectly & i draw the data to the PC Now 1-I want to know the maximum cable length without repeater and with repeater 2-i saw in the set PG/PC that i can connectup to 126 devices in one MPI network is it right or not thank you |
| 4/5/2006 1:25 PM | |
|
Joined: 8/25/2005 Last visit: 12/19/2025 Posts: 1162 Rating:
|
Hello magdy, Answering your questions:
Sabine |
Follow us on