(0)| 5/14/2009 5:53 PM | |
|
Posts: 7 Rating:
|
SO the with the actual configuration is not possible to achieve the communicattion between the systems, i must replace CP on the S7300 ? |
| 5/14/2009 6:16 PM | |
|
Posts: 7 Rating:
|
I am considering to use profibus , ido have the Em 277 for the S7200 and no doubts on hardware side .Do you by any chance have an example program? Regards |
| 5/15/2009 7:06 AM | |
|
Joined: 3/21/2006 Last visit: 12/31/2025 Posts: 10239 Rating:
|
Hello Look at How can you communicate data between the S7-200 and the S7-300 via PROFIBUS DP? Best regards Hristo Mihalev |
| 5/15/2009 1:16 PM | |
|
Posts: 5822 Rating:
|
Hello zulca, if I read the manual: S7-200 System Manual and here especially the Appendix A at the chapter EM277 PROFIBUS-DP Module Specifications I find the point User program Considerations. Here you will find the information that the S7-300 and S7-400 is able to access the S7-200 on the PROFIBUS interface by the use of XPUT or XGET functions, as long as the connection on the S7-300 / 400 is being done on MPI. Well, I have to admit that I see no reason why a S7-Connection on a PROFIBUS interface should not work also ... but I have to admit, I never tried it so far. So if you would like to do a try with a CP 342-5 on a S7-300 (DP interfaces on the S7-300 do not support S7 Client functions) or a PROFIBUS DP interface on a S7-400... I would really appreciate any information about your results. Best regards J_Bell |
| 10/20/2009 5:24 AM | |
|
Posts: 7 Rating:
|
I wanted to tell you that i was able to get the ethernet communicattion to work. Thaks |
Follow us on