(0)| 5/20/2009 8:25 AM | |
|
Posts: 12 Rating:
|
Hi all, Kindly tell me how to send & receive the data woth CP343-1 lean module via., TCP/IP. I have radio modem with TCP/IP communication. Reagrds, Sora |
| 5/21/2009 10:03 PM | |
|
Posts: 1742 Rating:
|
Hello, Firts you have to define a connection in Netpro. Here two examples http://support.automation.siemens.com/WW/view/en/22385024 http://support.automation.siemens.com/WW/view/en/22790099 I guess that you will have a transfer of data with variable length. Special attention is to be paid that TCP does not provide a mechanism for the detection the end of a message. The application must take this in count. Here an example where the ned of message is based on the detection of the character CR (Carriage Return). http://support.automation.siemens.com/WW/view/en/19033929 |
Follow us on