6/8/2009 6:07 AM | |
Posts: 691 Rating: (36) |
Please Check the System Parameters The Logical Device Name should be set as "Profibus" in Set PG/PC Interface AttachmentCheck.zip (78 Downloads) |
Last edited by: S7-Knight at: 6/8/2009 6:09 AM |
|
6/8/2009 7:23 AM | |
Joined: 9/27/2006 Last visit: 5/13/2024 Posts: 12257 Rating: (2667) |
Hello SPV; A ??? symbol in a WinCC animation means that you are not connected properly to the PLC registers you are trying to read. Are you using FMS connections? If so: How have you setup the WinCC PC for FMS comms? The S7 program, the WinCC channel? FMS (Field message Service) is very different than DP; only one "message" is transfered between participants, and you have to create it as a globalDB, dedicating it to FMS comms with a Communication option (see the following FAQ for details). Here is a FAQ that shows how you would have setup the FMS channel with a S7 PLC, using WinCC 5.1. You don't mention your version of WinCC or Simatic Net, but the basic principles should be quite the same whatever the version level is. http://support.automation.siemens.com/WW/view/en/14761448 Since theWinCC V. 7.0 system Description also mentions channels for FMS, you should have information available on the WinCC help files: WinCC also comes supplied with open communication channels such as PROFIBUS DP/FMS and OPC Hope this helps,Daniel Chartier |
Last edited by: dchartier at: 6/8/2009 7:26 AM |
|
6/12/2009 6:36 AM | |
Posts: 691 Rating: (36) |
Yes you got the Right Thing By Default WinCC takes CP_L2_1 as on board CP card (PC/MCI) AttachmentCheck.zip (54 Downloads) |
5/15/2018 2:19 PM | |
Posts: 2 Rating: (0) |
Dear All, I am also facing similar problem, here i have tried everythis as guided above.(PFA) Is there any other method possible to check and determine the problem. Attachmentimage.zip (25 Downloads) |
Follow us on