Industry Online Support
Technical Forum
6/13/2009 1:58 PM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306) |
Hello Paresh, Hello Junghans, Siemens HMI panels doesn't actas DP-Slaves when S7-PLC is Master. The only two cases the panel might be a slave are, 1- When you use DP direct keys. http://support.automation.siemens.com/WW/view/en/29339779 http://support.automation.siemens.com/WW/view/en/14668970 2- When you use HMI panel with S5 system. http://support.automation.siemens.com/WW/view/en/17053153 When you have multiple HMIs on the same bus then none of them is the only master (Class 2 Master)on the bus however I'm not quite sure of this and I hope someone can confirm or correct. I also recommend to look at this thread (regarding several HMIs on the same bus) and pay attention to the 2 replies of Fritz and J_Bell. Best regards. H-H |
7/25/2013 2:47 PM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating: (135) |
New question was splitted to Should I reserve communication resourses of CPU for HMIs ? Best regards O_Moderator |
Follow us on