(0)| 6/20/2009 9:16 AM | |
|
Posts: 3 Rating:
|
HOW TO CONFIGURE WINCC 7 TO CONNECT WITH 400H BY ETHERNET LAN DOUBLE? MANY TANKS FOR YOU HELP. |
| 6/20/2009 9:34 AM | |
|
Posts: 3 Rating:
|
OK. but is necessary two nos of card? is absoluty necessary to use a redconnect Software? tanks. |
| 6/20/2009 4:18 PM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hello, did you already seen the this previos tread from other experts? WINCC WITH 400H P.S.: one ot two CP on PC station doesn't change the philosophy how make redundant connection...it onlyimproves connection availibility (depending how you are going to build cable network) Regards |
| 6/21/2009 2:12 PM | |||
|
Joined: 1/4/2008 Last visit: 12/22/2025 Posts: 703 Rating:
|
Hello, another possibility is to use the two-port adapter CP 1623 instead oftwo CP 1613:
Regards Sydney |
||
| 6/22/2009 10:56 AM | |
|
Joined: 1/4/2008 Last visit: 12/22/2025 Posts: 703 Rating:
|
Hello CBo, although the CP 1623 can have at least two IP addresses (probably more as standard network adapter), you're right that for redundant cabling connection should be two of them used. I've read just the release information, haven't used it already. There is an information about two ports and possibility using with the S7-redconnect, but hasn't mentioned that it's still need to use two CPs Regards Sydney |
Follow us on