(1)| 6/26/2009 9:13 PM | |
|
Posts: 1742 Rating:
|
Hello, Just as an info. Siemens has a DVD with Technical Product Data for CAx Applications . Among other info, there are pictures in DWG format. More details here http://support.automation.siemens.com/WW/view/en/34066427 |
| 6/26/2009 10:11 PM | |
|
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
I did not find the picture which i am looking for on the above link, where can I download DVD from? |
| 6/27/2009 1:32 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello Lalit, Nice to replyto one ofyour threads again. the CAX DVD is not for free. However, the details you are looking forcan be found on manuals. For S7-300 systems, there are some good manuals that you should always have with you. 1 - SIMATIC S7-300 CPU 31xC and CPU 31x: Technical specifications. To know where the Profinet port is located for CPU 315-2 PN/DP, please look at page 27. 2- SIMATIC S7-300 CPU 31xC and CPU 31x: Installation. 3- S7-300 Instruction List. 4- SIMATIC S7-300 S7-300 Module data. (I think you already have this one In chapter 8, you will find all information regarding IM365. IM365 modules (Send/Receive)come with permanently connected cable(1m). So, there is no connectors. IM365 modules don't have DIP switches. For the CP341, Please look at chapter B (Connecting cables) in themanual. There's also a manual for Modbus slave driver. I hope you will find it useful. Best regards. H-H |
This contribution was helpful to
|
|
| 6/29/2009 3:14 AM | |
|
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
Hi H-H, Thanks for the info, I am still unable to find the info about IM-365 modules, I mean how those will be connected together, will that be a connector cable or we would need to wire it, how big the size of the connector, if you have those details, please reply.
|
| 6/29/2009 7:04 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello Lalit, The IM365 modules come preassembled. There's no connector. The cable is permanently connected so you can't take it out of any module. From S7-300 Module Data (Page 404), 8.4 Interface module IM 365; (6ES7 365-0BA01-0AA0) Special features of interface module IM 365: ● Preassembled pair of modules for rack 0 and rack 1 ● Total power supply of 1.2 A, of which up to 0.8 A may be used per rack. ● Connecting cable with a length of 1 m already permanently connected. Best regards. |
This contribution was helpful to
|
|
| 6/29/2009 9:21 AM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello Lalit, Here's a pictures of the IM356. When you will order it, you will recieve one package contans two modules (send) & (Recieve) modules with 1meter cable connected between them. Dimension of each module is WxHxD = 40x125x120 mm. Hope this info will help you. AttachmentIM pictures.zip (435 Downloads) |
|
Ayman Elotaify |
|
This contribution was helpful to
|
|
| 6/29/2009 4:42 PM | |
|
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
Thanks guys, I am fairly clear about, CPU & IM365 Modules, and I found the pin configuration of CP341, however I still did not find the modubus slave picture, how will it be connected to CP341, if some one of you has the picture of CP341- with the modbus slave driver please do post here. |
| 6/29/2009 5:28 PM | |
|
Posts: 261 Rating:
|
Hi lalit, If you already loaded the modbus master setup you can find the information under the Modbus Master pdf. The path is Start>simatic>documentation>English |
| 6/29/2009 7:32 PM | |
|
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
Still Can't find any picture how CP341 and dongle combination will look like.. |
Follow us on