(2)| 7/5/2009 3:33 PM | |
|
Joined: 10/7/2005 Last visit: 1/20/2026 Posts: 3054 Rating:
|
Hello Daniel your problem is most likely caused by the fact that the first download of your flex project to the Panel (the one that works) changes the settings for the MPI/DP transfer (I presume you use DP) and your USB MPI/DP adaptor is set to MPI. Here is an excerpt from the TP manual (which you can download from here): Transfer mode using MPI / PROFIBUS DP The bus parameters for MPI / PROFIBUS DP transfer, e.g. the MPI / PROFIBUS DP address of the HMI device, will be read from the project currently loaded on the HMI device. The HMI device uses the new MPI / PROFIBUS DP settings until you transfer another project to it. During the transfer of a project to the HMI device, the MPI / PROFIBUS DP settings will be overwritten with the values from the transferred project. You can thus edit the MPI / DP settings for the TP 177A irrespective of the project settings. Anyway, have a look through the manual which has more useful info on connecting anddownloading. I hope this helps |
|
Cheers |
|
| 7/6/2009 1:56 AM | |
|
Joined: 10/7/2005 Last visit: 1/20/2026 Posts: 3054 Rating:
|
Hello Daniel don't you hate when you think you have the "perfect" answer that explains what's wrong only to find out that it is probably something else? Anyway, have a look at the Control Panel of your TP177A. You'll find an "MPI/DP settings" icon (this handlesthe interface as far PLCcommunication is concerned and will be overwititen by your flex application settings) as well as a "Tranfer Settings" icon (this handles how you can download to the Panel and will be "reset" by an OS upgrade). Check the settings in both andmake espacially sure that the 2nd channel in the "Tranfer Settings"is enabled and set up for your download needs(e.g. MPI, DP, USB or Etehrnet for more powerful panels) and see also chapter 6.1 of the previous listed TP177 manual for more on this. I'll keep my fingers crossed that this helps in fixing the problem. |
|
Cheers |
|
| 7/6/2009 2:13 PM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hi Daniel..Nilsson, Let's hope you get an answer, that will help. Have you seen this link: http://support.automation.siemens.com/WW/view/en/19109408 The USB/MPI adapter is not released for transfer Best regards, Wizard |
This contribution was helpful to
|
|
Follow us on