(0)| 5/19/2006 8:25 AM | |
|
Posts: 102 Rating:
|
Hai Wizard, If say I am using ET200S I/O modules with S7 300 Master, is it possible Regards Shamsher |
| 5/20/2006 7:48 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Shamsher, The Wizard and Jacek D are right, when looking in the "S7-300 Instruction List CPU31xC CPU31x IM151-7 CPU BM147-1 CPU BM147-2 CPU" instruction handbook: http://support.automation.siemens.com/WW/view/en/13206730 on page 108 the information of OB83 is listed. But without OB83 is hot swapping also perfectly in a ET 200S station possible, the station stays in work when replacing the I/O-block when the "Module change during operation" or "Insert/Remove module" is put on. The only thing that must be cleared is that the addresses are called from the software and that they have to be blocked when detected with OB122. You might make a recognition over OB122 and OB82. [:o] In a ET 200M station it is also possible but you have to use then an active backplain. [:blush:] The function "Module change during operation" (or "Insert/Remove module") enables you to insert or remove modules during operation of the ET 200M rack and also for the ET 200S rack. [:P] "Module change during operation" - Configuration and system requirements http://support.automation.siemens.com/WW/view/en/1826766 gives more information about the hardware and software requirments for "Hot swapping" with a S7-300 system. [8)] |
Last edited by: Late at: 5/20/2006 7:53 PMHmmm... another error in typing Last edited by: Late at: 5/20/2006 7:51 PMSome errors in typing cleared I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
| 10/19/2015 5:15 PM | |
|
Posts: 4758 Rating:
|
New question published by AutoGen_417353 is split to a separate thread with the subject 315-2dp software redundancy support Hot Swapping?. Best regards |
Follow us on