(0)| 9/2/2009 1:26 PM | |
|
Posts: 56 Rating:
|
Dear Friends, How i can able to use with S7-200 CPU (4 nos) with one no of WINCC SCADA and External MODBUS DCS master. Regards, Raj |
| 10/13/2009 12:43 PM | |
|
Joined: 7/13/2009 Last visit: 11/27/2025 Posts: 137 Rating:
|
Hello Anguraj, There are some third party OPC servers available which can directly communicate with S7 200. So that WinCC as well as DCS both can able to communicate with OPC u implement communication between S7 200 and third party OPC server. Then u can acess all 4 S7 200 stations to WinCC as well as DCS through common protocal. You can also see the link bellow, Regards, Manjunath |
|
Thanks and Regards |
|
Follow us on