(0)| 9/4/2009 12:12 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Seems you don't have correct installation files. Did you use the same installation files with success before? If you are trying to install directly from CD, try first to copy installation files into hard disk and then start... Regards |
| 9/4/2009 6:49 PM | |
|
Posts: 133 Rating:
|
With SIZER V3.1 the file for the CAD drawings are seperate but required with the default installation settings. If you do not insert the CAD folder in the correct directory you will get the error you described. It is possible to install V3.1 without the CAD drawings but you must go into the Custom setting of the dialog page and deactivate the dimension drawings. a) First download the zip-file „SIZER_V31.zip“ and unpack it. If you do not want to install the dimension drawings (CAD Creator)in SIZER skip to point c and see note belowSIZER installation without dimension drawings. b)Next for installation of CAD drawingsdownload the zip-file „SIZER_V31_CAD.zip“. This zip-file contains the file „Data2.cab“. This file must be copied resp. unpacked into the subdirectory ...\SIZER after executing the point a). Then the file „Data2.cab“ (667886 KB) must be placed in the same directoryas the file „Data1.cab“ (401083 KB). Check that you are in the correct directory by the file size of Data1.cab as there are two directories with this file name. The dimension drawings are preset in the setup now. c) Start the program setup.exe in the highest level directory. *note if you do not want to install the dimension drawings into SIZER V3.1 you only need the first zip file but you must choose custom installation and deselect dimension drawings.SIZER without dimension drawings Download the zip-file „SIZER_V31.zip“, unpack it and then start the program setup.exe. Important Note: In the setting "Custom" in the dialog page "setuptype" of the setup the dimension drawings must be deactivated. |
| 9/7/2009 3:57 AM | |
|
Joined: 9/6/2007 Last visit: 1/21/2026 Posts: 81 Rating:
|
Ya...my problem is in the drawing diemension. Thanks.... Another question: Our project's CAM profile wants to use "Modified sine curve". Can SIZER help me to calculate this curve "MSC"and choose motors ? I try to use the SIZER and I just see the triangular and trapezoidal curve. CanSIZER useother curves ? Angus. |
| 6/10/2010 8:14 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
can you give download links?? |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
| 6/10/2010 8:22 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, You chould contact with Siemens repr. From there you could receive. Best regards, Hristo Mihalev |
Follow us on