(0)| 9/11/2009 11:36 AM | |
|
Posts: 261 Rating:
|
Seems the link may help you. The attached pdl in 6.2 you can upgrade it to 7.0 With best regards ddg |
| 9/12/2009 8:19 AM | |
|
Posts: 261 Rating:
|
Hi Rahul Sayre, Yes you can change the path. Option 1: If you open the script where it is clearly mentioned that “'If required Replace <path> with the real path of the file "E:\Wincc_with_vb\Excel_Test".” So you can change from the script. The change is static. Option2: If you want to configure the path from Wincc (Dynamic) then you have to create the excel file from HMI. In this attached sheet I give you the example program how to create excel file from HMI? Note: You have to create two tags (Text tag 8 bit character set) to give the file path and sheet name. 1. Tag name: File_name 2. Tag name: Sheet_name Another Two Buttons are also added which are having with the dynamic path. Hope it helps you. With best regards ddg AttachmentRef.zip (384 Downloads) |
Last edited by: ddg at: 9/12/2009 8:19 AM |
|
| 9/14/2009 7:23 AM | |
|
Joined: 2/24/2009 Last visit: 9/5/2025 Posts: 116 Rating:
|
Dear Sir, Thanx for reply . regards, Rahul |
| 9/14/2009 8:44 AM | |
|
Posts: 261 Rating:
|
You are welcome |
Follow us on