(0)| 10/15/2009 9:29 AM | |
|
Posts: 289 Rating:
|
Hello Shary, You can record curves containing different internal parameters (pressure, temperature, exact date/time, inputs, outputs) with the help of Data Log Wizard. It's pretty easy to use. The data can be stored on an external memory card (for S7-200) and can be downoladed (csv. format) using S7200 Explorer. https://support.automation.siemens.com/WW/skm/frameset.asp?url=%2FWW%2Fllisapi%2Edll%2F27207658%3Ffunc%3Dll%26objId%3D27207658%26objaction%3Dcsopen%26skm%3D1%26siteid%3Dcseus%26lang%3Den&Query=S7%2D200+Explorer&SearchArea=downl&id=27207658&F11Marker=true&siteid=cseus&query2=&modelled=&lang=en Depending on how fast you write the data on the memory card you can get a very detailed reprezentation of the values. Max memory card for S7-200 as far as I know is 256K. I atach for you a small excel doc with a sample of such recording. Attachmentsample.zip (280 Downloads) |
Follow us on