(0)| 10/22/2009 9:05 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi Delphoe , i need a start point, so i assume you have nr.3 station: 1 ES, 1 OS server and 1 OS client. In Enginnering station you have to insert in your project nr 3 "SIMATIC PC Station" in Simatic Manager->Component View. 1) in ES station -> HW configuration need insert your comunication card 2) in OS Server station -> HW configuration need inseert "WinCC Aplication" and comunication card 3) in OS Client station -> HW configuration need inseert "WinCC Aplication Client" and comunication card 4) open "OS server" and "generate server data" (or just right click on OS server and select generate server data), then open "OS Client" and "import server data generated". 5) create connection between ES<-->AS and OS Server<-->AS 6) download all PC station configuration, all HW & SW and comunication and each OS Project it will be ready Comunication between server<-->client has estabilished by "server data" generated in OS Server and imported in OS Client Hope can help reagrds |
Follow us on