11/4/2009 4:55 PM | |
Posts: 133 Rating:
|
Hello, As a display on the cabinet door it works fine with S120 multi-axis systems but it was designed more for a single drive application (i.e. G130, G150, S150). For applied machines most people finda HMI like the TP170 (class II Profibus direct connect to the CU320) a more optimal solution from price and functionality. The screens are easy to design and can be tailored for the machine. If you are commissioning a multi-axis system STARTER on a PC is aten times easiler. Also see post below: /tf/WW/en/Posts/15224#top |
Follow us on