(2)| 11/11/2009 8:35 PM | |
|
Posts: 14 Rating:
|
Hi Tomy, In catalog ST-70 2009 (on page 486 of the PDF), the following is statet: IM 153-1 Standard The IM 153-1 is one reasonably priced version that is best suited for most applications in the manufacturing environment. It permits the use of up to eight S7-300 I/O modules. IM 153-2 High Feature For higher requirements in manufacturing technology, such as the use of F-technology or the highest performance in conjunction with clock synchronization, the IM 153-2 High Feature is available. This IM is also designed for use with the PCS 7 in the field of manufacturing applications. This IM can be redundantly used and supports typical functions as they are required in the control field. These include, for example, clock synchronization or time stamping with an accuracy of up to 1 ms.
|
Last edited by: Tim de Bruin at: 11/11/2009 8:37 PM |
|
This contribution was helpful to
|
|
Follow us on