(1)| 11/12/2009 10:36 AM | |
|
Posts: 66 Rating:
|
Dear All, 1) Error while uploading I am using Microwin V4.0.0.81 softwareto upload S7 224 CN CPU. While uploading it shows the error message (The project file contains one or more old constructs that version 4.x does not support) and blocks the uploading. What shall I do? I attached bmp file for more details. 2) If communication port assigns for another function e.g.RS 485 or port assigns for another functions to communicate other devices then afterdownloading should I go onlineand make changes. (Device having only one port) If this will not possible then what the another procedure to test the system? Gaurav AttachmentError message while uploading.pdf (1098 Downloads) |
| 11/16/2009 9:14 AM | |
|
Posts: 2930 Rating:
|
Hi, the EM277 also support lower baudrates. Also the PPI-cables can be used with the EM277. I hope this helps. |
| 12/2/2009 2:29 PM | |
|
Posts: 2930 Rating:
|
Hi, with the actual version of MW V4.0 SP7 you can always upload from a CN PLC, independant form the selected language. regards |
Follow us on