(0)| 11/18/2009 2:26 PM | |
|
Posts: 17 Rating:
|
Hi Mazdak, Galvanic isolation is a way of isolating elctricaly inputs from functional parts of the module, so the signal is readed by the module, but it's protected against overvoltages or overcurrents from field. There is no electric current flowing directly from one section to the next. Information is still exchanged between the sections by other means, however, such as optical, Optical isolation is a way of Galvanic Isolation, like optocouplers (when you have current in the transmitter, its transmit a light beam wich excites a receiver, allowing the current to pass trough it, so there is no current pass between transmiter and receiver). Best regards Patricio Novotny SILOGIC Ingeniería y Automatización Bolívar 284 Piso A - (B1704BKF) Ramos Mejía - Bs. As. - Argentina tel. 54 11 4656 4349 fax. 54 11 4464 5844 cel. 54 11 15 6058 0699 www.silogic.com.ar |
| 11/23/2009 2:25 PM | |
|
Posts: 17 Rating:
|
Hi Mazdak, You should use fuses in each digital output to protect it agains't short circuits. Best regards, Best regards Patricio Novotny SILOGIC Ingeniería y Automatización Bolívar 284 Piso A - (B1704BKF) Ramos Mejía - Bs. As. - Argentina tel. 54 11 4656 4349 fax. 54 11 4464 5844 cel. 54 11 15 6058 0699 www.silogic.com.ar |
Follow us on