(0)| 12/5/2009 6:15 AM | |
|
Posts: 11 Rating:
|
i want to communication between two s7-400 & one hmi................anybody know the configuration .........help me................. |
| 12/5/2009 6:40 AM | |
|
Posts: 382 Rating:
|
Hello, Is your two S7-400 a H-system? Is your one HMIreferring to MP or OP or TP or PC using WinCC? And the types ofcommunication methods you are looking for? Maybe these cangive yousome help 1] MP377 WITH CPU412-3H CONTROLLERS 2] COMMUNICATION OF S7 400 H CPU WITH MP 377 THROUGH ETHERNET LINK 3] How do you connect an operator panel (WinCC flexible) to an H system (S7-400H) about MPI or PROFIBUS? 4] How can you connect an operator panel directly to an H system without using repeaters? 5] WinCC 7.0 and ethernet connection to S7-400 by CP 1613 A2 card Good luck with regards, howcome |
This contribution was helpful to
|
|
Follow us on