Industry Online Support
Technical Forum
12/18/2009 1:46 PM | |
Posts: 28 Rating: (1) |
Hi. I need to do the next: From a VBS Script in a click button I need to put 1 in an individual bit of a DWORD Variable. Thanks
|
12/18/2009 4:34 PM | |
Joined: 4/19/2008 Last visit: 6/6/2024 Posts: 1525 Rating: (159) |
Hi DavidSG, Please find the C-Script file. Sorry but I have only C Script. in this you have to give the Tag & Bit No. & one more addition is that if you Click on Same button it will Invert the status Like First time you click on Button Bit change to 0 to 1 2ndtime you click on Button same Bit change to1 to 0. You can used this Script for Byte, Word & DWord Also. AttachmentSc.zip (254 Downloads) |
Last edited by: Ammy at: 12/18/2009 4:35 PMAmmy |
|
12/21/2009 9:01 AM | |
Posts: 63 Rating: (39) |
i download your c function but when i open it, shows me a message box for password pls send a password from mayank AttachmentSc.zip (107 Downloads) |
12/29/2009 10:34 AM | |
Posts: 28 Rating: (1) |
Thanks to all. I need VBS code because I put this in a button of an MSgBox and I can't know how to show an msgbox in C. |
Follow us on