(0)| 12/23/2009 9:28 AM | |
|
Posts: 41 Rating:
|
Hi all, When i open my multiproject , error message come.( "Internal data structure error") error message is attached as a screenshot. 1. what is reason behind this error? 2. How to resolve this error? 3. now due to this error , i am not able to download changes in CPU. i have to download whole progran atleast once . 4. what will happen , if i download same program to cpu.is it leads to fault in CPU or it will work? 5. my plant is running....so pls guide me , what should i do now? thanks in advance. Rahul Attachmentproject open error.pdf (356 Downloads) |
| 12/23/2009 6:13 PM | |
|
Posts: 2661 Rating:
|
Hi Raul0905, The project is corrupted. See the error code 257:90 in the attached document. The remedy is to do a Save As with Reorganization (slow) of the project. But this may require a plant stoppage. Do you have backup of the project? Regards AttachmentSTEP7_ErrorCode_engl.pdf (419 Downloads) |
Follow us on