1/18/2010 3:36 PM | |
Joined: 9/27/2006 Last visit: 5/28/2024 Posts: 12257 Rating: (2668) |
Hello guys; Ir might be worth looking into the Ethernet //IP driver available in WinCC v. 7.0. It states that it is designed for Controllogix, but FlexLogix uses the same programming software (RSLogix 5000)and environment (I am thinking of RSLinx), so the drivers should be compatible. Worth a try anyway, no? Have a look at the WinCC 7 system communications manual: http://support.automation.siemens.com/WW/view/en/37436836 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
1/28/2010 2:40 AM | |
Posts: 28 Rating: (0) |
Hi, |
Follow us on