(0)| 1/27/2010 3:36 AM | |
|
Posts: 4 Rating:
|
Dear Nemo. I have a similar problem, I´ll explain you. at beginning I convert a protool project from Protool --> WinCC flex 2008. automatically choose an OP177. I perform tags, screens, alarms, etc... and I start the RT... everything is OK. then... I change a device to MP277 in order to usegraphics and so on. this time when I start RT I got the next message (error message.bmp), so I delete temp files by Options\Delete Tem Files. Later. Compiler\Rebuild all.. and thats the same. I have this version installed. (WinCCFlex2008SP1HF3.bmp) finally if I try to open an older project designed on WinCCflex 2007 for example I got the message about incompatible or beta version of wincc flex.(error message old project.bmp) I try to uninstall SP1 and HF3 but its imposible the process is aborted. I just can repair the software. Thanks a lot in advance!! AttachmentWinccflex2008.zip (987 Downloads) |
Last edited by: O_Moderator at: 1/27/2010 9:44 AMnew subject after splitting from /tf/WW/en/Posts/10404#top |
|
| 1/27/2010 9:27 AM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9105 Rating:
|
Dear DLuna_GDL, Have you tried to Reset WinCC flexible to original status of last installation: How can you reset WinCC flexible to the original status of last installation? Perhaps this link, might help in uninstalling WinCC flexible and install it again: What can cause the installation to abort or prevent successful starting of WinCC flexible? Best regards, Wizard |
| 7/28/2011 8:06 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Perhaps if they send you another backups followed http://support.automation.siemens.com/WW/view/en/21896449 ...if we assumed the probelm is in backup files. best regards, Hristo Mihalev |
| 7/28/2011 9:07 AM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9105 Rating:
|
Dear Richvida3, What is the exact version of WinCC flexible 2008 you are using? (including Servicepacks and Updates) The project might be programmed with a newer version then you have. Here you can download Service pack 2 for WinCC flexible 2008: Service Pack 2 for WinCC flexible 2008 and the latest update: Update for WinCC flexible 2008 Service Pack 2 Best regards, Wizard |
| 2/5/2013 5:08 PM | |
|
Posts: 3 Rating:
|
I am having the same problem. I have files that were worked on by another, and when I try to open them I get the same error above. Attached you can see the error, and my version information. The error says SP1, and I am up to SP2.I have used the cleanup utility to remove and reinstall, but this did not help. I have confirmed that the software is functional. I am able to import the original project from ProTools, but it does not contain the modifications that I need, which are in the other file(s). The error message does not make sense to me, unless it is not accurate with the SP information. The numbers in the error message do not seem to correlate with any of the numbers in the information boxes. Thanks for your help. AttachmentWinCC Issues(1).zip (488 Downloads) |
Last edited by: O_Moderator at: 2/6/2013 1:33 PM |
|
| 2/7/2013 1:22 PM | |
|
Posts: 3037 Rating:
|
Hello, You can see more information in the following links. /tf/WW/de/Posts/75218 /tf/WW/de/Posts/64648 /tf/WW/en/Posts/57328#top Tweety |
| 12/31/2014 2:53 PM | |
|
Posts: 1 Rating:
|
svp comment resoudre ce probleme sur wincc fexible le projet a ete cree avec une version incompatible ou une version beta de wincc flexible merci |
| 3/23/2015 9:54 AM | |
|
Posts: 1 Rating:
|
hi , i have the same problem and i have wincc flexible SP3 and also the same . but i like to mention you the program from chine , and i am worried that not the same type of programe
|
This contribution was helpful to
|
|
Follow us on