(0)| 3/31/2010 1:16 PM | |
|
Posts: 118 Rating:
|
Dear Ahmed Majeed, I hope my answer is not that late If you want to have data transfer from S7-300 CPUs to the hmi PC over GSM or GPRS then SINAUT ST7 Telecontrol would bea good solution for you. You need SINAUT hardware at the S7-300 (TIM-Modules) and the modem. (GSM or GPRS) Then you need SINAUT ST7cc which is an Add-on WinCC for your pc, plusa modem (dial up or gsm) for telephone lineor if you use IP-based network like GPRS at the remote CPUs then you need a DSL modem at the pc. You also need the SINAUT ST7 Configuration software to configurate your connections. Have a look at the following links where you can find schemas and description of these solutions. GPRS Solution (cost-optimised) http://support.automation.siemens.com/WW/view/en/38698845 GPRS Solution wich high data security (see 2nd picture and volume 2) http://support.automation.siemens.com/WW/view/en/23810112 FAQ, How to configure the GSM Modem for SINAUT ST7 (Telephone /GSM solution) http://support.automation.siemens.com/WW/view/en/29586028 More examples about SINAUT ST7 (Here you can find Info on how to conigure connections with SINAUT ST/ etc) http://support.automation.siemens.com/WW/view/en/22340652 |
| 3/31/2010 1:30 PM | |
|
Posts: 118 Rating:
|
Dear Ahmed Majeed, I forgot all about it.There is also another solution , which might be interesting for you and more cost-effective. Have a look: Wireless Data Communication based on GPRS between S7-300 stations and SINAUT Micro SC Server: http://support.automation.siemens.com/WW/view/en/27038105 |
Follow us on