(0)| 3/31/2010 5:46 AM | |
|
Posts: 13 Rating:
|
I am Kiran from Pacific central teknik. I used the Siemens system CPU315 2PN-DP to our one project Wyeth. In this project I have not established the communication between third party CP-342-5DP to our CPU 315-2PN DP. I connected the profibus link between CP342-5DP & CPU DP port. Required H.W configuration I have done but still communication not established. So how can connect the CP342-5dp to my CPU. Please give me the support on this. It’s very argent. Checked my H.W. Also. Detail of CP parameter as below.Third party send the 72 byte data & receive the 14 byte data.( AS per addr. List provided by Customer) Communication processor cp342-5dp DP address:12 Mode of operation: dp slave passive Baud rate: 1.5 MBit/s, Bus profile: std, highest profibus addr:126, Max data to transfer:250 byte. Regards, Kiran Sonar. Attachmentref.zip (272 Downloads) |
| 3/31/2010 8:04 AM | |
|
Joined: 8/25/2005 Last visit: 1/14/2026 Posts: 1162 Rating:
|
Hello kiranPCT, please have a look at the following page: SIMATIC Net Quick Start There you will find an example. At the side of the CP342-5 CPU you have to programm the FC's DP_SEND and DP_RECV. Are they there? Good luck Sabine |
| 3/31/2010 9:40 AM | |
|
Posts: 13 Rating:
|
Dear sir, thanks for reply. you send me the 2 .exe file but i can't open this file. which type of this file? still i suffering the same problem. kiran sonar |
| 3/31/2010 3:29 PM | |
|
Posts: 13 Rating:
|
Dear, Thanks for co-operation. I have gone through all your attachment . for this I understand that both hard ware configuration required in one project. Am I right? In previously I configured only Master PLC configuration. May be that time I cannot connect CP-342-5DP to MY CPU 315-2PN DP.I will change the Configuration and check again. I known witch modules used in Slave System.(Third party). Please check the attachment, I have only this much information from Customer side. Regards, Kiran Sonar. AttachmentCP Information & ADDR. List.pdf (350 Downloads) |
| 4/5/2010 8:54 AM | |
|
Posts: 13 Rating:
|
Hi, AS per your information regarding CP communication I have checked all Configuration between DP Master and DP slave. But still my problem is not salved.I have download the GSD file of CP-342-5DP. After downloading this file I access following path Additional Field Devices > I/O > SIMATIC. Before this path not shown in my PLC software. In this path CP-342-5 Cu Slave shown in hardware library. The GSD file type is SIEM80d6.GSD. I have only configured the Master system and add the CP342 5Dp on probibus network. Still SF & BF coming in my system. I cannot communicate third party Slave to my CPU. Please see the attachment of the error coming on plc. Same error came in every configuration. Means suppose I select the CP slave from following path in hardware Prfibus DP/Simatic/CP345-5DP in this type GSD file of CP-342-5DP is SIEM80d6.GSE. Also I configured Slave Station in my project. I select CP from Prfibus DP/configuration station. What is mean of CPU 342-5 Cu.? Please check. Attachmentplc error.pdf (339 Downloads) |
Follow us on