(0)| 4/16/2010 11:30 AM | |
|
Posts: 101 Rating:
|
The Masterdrive is still a current Siemensproduct and even if it is 10 years old, the new components are all backwards compatable. As you have a frame size F (chasis type)I would advise on replacing the damaged components, much easier and cheaper than replacing the whole drive. What is the problem with the drive? As it is an Atlas Copco compressor, I suspect F25, 26 or 27 which would indicate an IGBT problem. The manual can be found here: http://support.automation.siemens.com/WW/view/en/23657884 |
| 4/28/2010 6:43 AM | |
|
Posts: 80 Rating:
|
Thanks Everybody, Thax for suggestion |
| 9/10/2019 1:07 PM | |
|
Joined: 3/25/2008 Last visit: 12/18/2025 Posts: 230 Rating:
|
What type of compressor it is. it is not easy to replace 6SE70 with 6SE6440 |
Follow us on