(0)| 6/6/2010 6:25 AM | |
|
Posts: 7 Rating:
|
Hi Mark, Same thing happened with a brand new pasCC projectwith one picture and the wizard file! Dont you think its may be because of Some hotfixes or something? |
| 6/7/2010 10:21 AM | |
|
Joined: 10/9/2007 Last visit: 12/18/2025 Posts: 1295 Rating:
|
Hi Soroush In the attached pictures you can see howPASCC controls the compatibility keys. When you import from the Wizard, PASCC writes in the internal WinCC variable the actual compatibility key from the PXD file, exported from PAS (picture Compkey from PXD). When PASCC connects to PAS, it reads the compatibility key from PAS (picture Compkey from Sicam) and compares them to the internal variables. You can see the value in PAS Configuration (picture Compkey in Configuration). Also you can open the PXD file and see the value. Are these values the same? After you export the PXD file, stop and start the HMI connection in PAS-Operation. Don't stop only the Interface, but the first level (default name is PAS CC). Mike J AttachmentCompkey.zip (302 Downloads) |
|
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on