(0)| 6/9/2010 8:04 PM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, Function blocks (FBs) are equipped to send requests to and receive requests from the VS 710 : FB 103: SEND function block for transmitting requests to the VS 710 . FB 105: RECEIVE function block for receiving acknowledgment messages and measured values from the VS 710. Use the installation program on the ProVision CD (STEP7\DISK1\setup.exe) to install a separate VS 710 library in STEP 7. The libraries contain (among other things) a SEND function block, a RECEIVE function block, an SCL example and some STL examples for these function blocks, and some variables tables (VAT). All source files are on the ProVision CD in the STEP7\SOURCE directory. Look for more at PROFIBUS-DP Vision Sensor SIMATIC VS 710Best regards,Hristo Mihalev |
Follow us on