(6)| 6/17/2010 9:02 AM | |
|
Joined: 9/18/2006 Last visit: 12/8/2025 Posts: 596 Rating:
|
Hi. You try to make so: 1) To change 38000 2) To create NC-archive 3) To load this NC-archive. Best regards. |
| 6/17/2010 10:21 AM | |
|
Posts: 2964 Rating:
|
Hi... Anyentry in Axis MD parameter38000 will cause "Memory Re-organization". So what you should means in that condition take a NC archive bacup and give an NCK reset, then reload the NC archive backup which was taken in memory reorganized condition. Now you should able to see your compensation data. I have write up for LEADSCREW PITCH ERROR COMPENSATION you can check the same. Hope this infromation will be useful to you..... Ekalavya AttachmentLPEC.pdf (1093 Downloads) |
This contribution was helpful to
|
|
| 6/19/2010 7:53 AM | |
|
Posts: 159 Rating:
|
Machine is now compensated!!!! Thanks for the help guys!!! Craig. |
Follow us on